ТОО "Эндресс+Хаузер (Казахстан)"
ТОО "Эндресс+Хаузер (Казахстан)"
ул. Зеина Шашкина 24, БЦ "K-Plaza", 4 этаж
050040, Almaty/Алматы
Казахстан
Component cleaning is an important part in manufacturing industrially produced components. When done correctly, it makes a critical contribution to robust and reliable function. Here, customers can rely on the precision and expertise of Swiss market leader Borer Chemie AG and the ultrasonic field devices Teqwave F, I and T from Endress+Hauser.
The close cooperation of Borer Chemie AG and Endress+Hauser ensures that customers have an efficient and consistent process for their products.
For requirements involving concentration measurement and bath monitoring, users of deconex® products in combination with the real-time analysis of Teqwave have the certainty of relying on a dependable and up-to-date method.
As in the upstream manufacturing steps, precision is also required in component cleaning. Only the right combination of cleaning agent and process ensures the necessary cleaning effect and optimum surface quality. For this, it is important for the concentration of the cleaning agent to be kept at the best possible level for the entire duration of the process.
With the versatile ultrasonic-based meters Teqwave F, I and T, Endress+Hauser offers the respective suitable solution for concentration measurement in real time. The Borer Chemie AG test and training center in Zuchwil, Switzerland, is one-of-a-kind in Europe. This facility allows customers to test deconex® cleaning agents and processes as well as high-precision concentration measurement with Teqwave.