ТОО "Эндресс+Хаузер (Казахстан)"
ТОО "Эндресс+Хаузер (Казахстан)"
ул. Зеина Шашкина 24, БЦ "K-Plaza", 4 этаж
050040, Almaty/Алматы
Казахстан
This white paper explains how self-calibrating thermometers can be used in hygienic process engineering. It details theory and practice as well as application examples.
The self-calibration method uses the Curie temperature (Tc) of a reference material as a built-in temperature reference. Self-calibration is performed automatically when the process temperature (Tp) drops below the nominal Curie temperature (Tc) of the device.
The electronics unit detects this change automatically and simultaneously calculates the deviation of the measured Pt100 temperature from the known Curie temperature, which is a physical fixed point.